SLVA888C April 2017 – January 2021 TPS65987D , TPS65988
This device has multiple GPIOs which could be used to assign PD events from the device configuration tool. These GPIOs supports multiple event options to indicate various states. It can take inputs from the system to make appropriate decisions. All the unused GPIOs should be left floating in the hardware. Some of the GPIOs have specific features and should be used accordingly. Refer to the TPS65987DDH schematic checklist in the Appendix of this document.