Use the following instructions to evaluate the thermal performance of TPS25985EVM:
Configure the Jumper J6 position to desired reference voltage (VIREF) for overcurrent protection and active current sharing as mentioned in Table 4-3. The "3-4" position of the jumper J6 is selected in this experiment, which makes VIREF as 1 V (typical).
Configure the jumper J4 in a suitable position to set required circuit breaker threshold (IOCP) as per Table 4-3. Both the "1-2" and "3-4" positions of the jumper J4 are selected in this experiment, which makes IOCP as 170 A (typical) with VIREF as 1 V (typical).
Set the input supply voltage VIN to 12 V and current limit of 110 A.
Connect the power supply between VIN (Connector T1) and PGND (Connector T3) and enable the power supply.
Now apply a load of 100 A (DC) between VOUT (Connector T2) and PGND (Connector T3) for half an hour or more to reach the thermal equilibrium point.
Capture the thermal image of the EVM or monitor the voltage at TEMP (TP14) pin using a digital multimeter. Voltage at the TEMP (VTEMP) pin reports the maximum die temperature between two (2) TPS25985 eFuses, which can be obtained using Equation 1.
Equation 1.
Figure 5-19 shows the thermal performance of TPS25985EVM with two (2) TPS25985 eFuses in parallel.
Figure 5-19 Thermal Performance of TPS25985EVM (VIN = 12 V, IOUT = 100 A, TA = 25 ºC, and no external air flow)