5.10 PROCHOT# Implementation Using General-Purpose Comparator
Use the following instructions to implement PROCHOT#™ functionality using in-built general-purpose comparator:
Configure the Jumper J3 to an appropriate position to obtain required overcurrent blanking period (tTIMER) as per Table 4-3.
Configure the Jumper J6 position to desired reference voltage (VIREF) for overcurrent protection and active current sharing as mentioned in Table 4-3.
Configure the jumper J4 in a suitable position to set required circuit breaker threshold (IOCP) as per Table 4-3.
Connect the CMPM pin (TP15) to the output of LDO, U4 (TP36) and adjust the values of R26 and R27 to make the voltage at TP36 to be 80% of VIREF.
Connect CMPP (TP17) with IMON (TP27).
Set the input supply voltage VIN to 12-V and connect the power supply between VIN (Connector T1) and PGND (Connector T3).
Now apply a transient load in the range of 0.7 × IOCP < ILOAD < 0.95 × IOCP (as example) between VOUT (Connector T2) and PGND (Connector T3) for a specified time duration, as example 20-ms, which is less than 2 x tTIMER decided by using jumper J3.
Observe the waveforms of CMPM (TP15), CMPP (TP17), CMPOUT (TP21), and load current using an oscilloscope.
Figure 5-16 shows the experimental waveforms of PROCHOT#™ implementation on the TPS25985EVM eFuse Evaluation Board.
Figure 5-16 PROCHOT#™ Implementation on TPS25985 eFuse (VIN = 12 V, RIMON = 1.1 ∥ 1.1 kΩ, RIREF = 40.2 kΩ, VCMPM = 0.8 V, and IOUT Ramped from 70 A to 95 A then 70 A within 20 ms)