SSZT740 April   2018 CC3120

 

  1.   1
  2.   2
    1.     3
    2.     The Process toward Failure
    3.     Early Indicators of Failure
    4.     From Regular Inspections to Continuous Condition Monitoring
    5.     Vibration Condition Monitoring
    6.     Conclusion
    7.     Additional Resources

Many motors and pumps are critical in factory production; a functional failure might cause a complete line stop. To avoid this, there are usually extensive preventive maintenance plans in place that require work at regular intervals. These plans are based on lifetime statistics and not on the actual condition of the equipment.

If you know the condition of the equipment, you can reduce maintenance costs as well as the risk of an unexpected breakdown. Using this knowledge to schedule repair and replacement is called predictive maintenance.

The Process toward Failure

You can understand the condition of equipment because there is a process leading to its final functional failure (as illustrated in Figure 1). Usually, this failure process takes time (for example, think about wear or contamination as a source of failure).

GUID-FAC3DB97-139D-4760-8F33-20BBCFCCB355-low.png Figure 1 Failure Process and Cost to Repair

Early Indicators of Failure

Fortunately, you do not have to wait until the equipment is broken – because there are early signs and signals that indicate a potential failure. The time from being able to detect a potential failure (P) until the actual functional failure (F) occurs is known as the P-F interval. Some indicators for motors with their corresponding P-F intervals that you can find in the literature include:

  • Oil analysis (months).
  • Vibration (weeks to months).
  • Power (weeks to months)
  • Thermal image (weeks).
  • Audible noise (days to weeks).
  • Heat (days).

Obviously, the earlier you can detect a potential failure, the more time you have to react, plan and execute equipment maintenance (Figure 2).

GUID-72FD7406-E6CB-4A5A-978A-64208AB5A2F2-low.png Figure 2 P-F Curve – Potential Failure to Functional Failure

From Regular Inspections to Continuous Condition Monitoring

Another factor you must consider is the inspection interval: How often do you check for signs of potential failure? A longer inspection interval reduces the time you have to plan and execute the repair. In the worst case (as shown in Figure 3), you might have checked the condition just shortly before observing the potential failure, so when you detect the problem at the next inspection interval, the time to schedule and execute the repair is shorter than the P-F interval minus the inspection interval.

The best method would indicate a potential failure as early as possible while keeping the inspection intervals as short as possible; in other words, observing failure indicators continuously.

GUID-44CA72FB-71BE-409F-B757-076CEB5E2A1D-low.png Figure 3 Inspection Interval

Vibration Condition Monitoring

Changes in vibration are very early indicators for potential failure; in addition, it is simple to measure vibration continuously. The Reference Design for Wireless Condition Monitor for Motors and Pumps Using Multi-Axis Vibration is an example for such a vibration sensor. It uses an analog three-axis accelerometer that is measured by the precision analog-to-digital converter (ADC) in the MSP432P4. The measured data is processed in the sensor node by generating a fast Fourier transformation of it. The resulting frequency-domain data determines changes in the vibration patterns but also reduces the amount of data transmitted wirelessly via Bluetooth® low energy to a gateway, smartphone or tablet.

As shown in Figure 4 on-site operators can use the data from the sensor directly for diagnostics and troubleshooting. In the cloud, you can store the data and perform further analysis on the basis of previously captured data.

GUID-4434AA1A-6944-435F-8689-EA5AFE57E927-low.png Figure 4 Vibration Condition Monitoring Setup

Conclusion

Continuously monitoring the vibration of critical assets like motors and pumps in factories provides an early indication of a potential failure and enables you to plan the maintenance of equipment based on its actual condition, thus saving money. Adding a wireless sensor that pre-processes the data is an easy and low-cost way to add this functionality to motors and pumps.

Additional Resources