SWRA772 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
  5. Running the Bluetooth Code
  6. Demo Application
    1. 3.1 Device 1 (Server) Setup on the Demo Application
    2. 3.2 Device 2 (Client) Setup on the Demo Application
    3. 3.3 Initiating Connection from Device 2
    4. 3.4 Identify Supported Services
    5. 3.5 Data Transfer Between Client and Server
    6. 3.6 Multiple SPPLE Connections Guide
  7. Demonstrating SPP LE on an iOS Device with the LightBlue App
    1. 4.1 LightBlue Overview
    2. 4.2 SPP LE Service Overview
      1. 4.2.1 Characteristics
  8. LightBlue as the Client/SPPLEDemo as the Server
    1. 5.1 Connecting the Devices
    2. 5.2 Enabling Notifications
    3. 5.3 Sending Data from LightBlue/Receiving Data in SPPLEDemo
    4. 5.4 Sending Data from SPPLEDemo/Receiving Data in LightBlue
  9. LightBlue as the Server/SPPLEDemo as the Client
    1. 6.1 Connecting the Devices
    2. 6.2 Sending Data from LightBlue/Receiving Data in SPPLEDemo
    3. 6.3 Sending Data from SPPLEDemo/Receiving Data in LightBlue
  10. Application Commands
  11. General Commands
    1. 8.1 Help (DisplayHelp)
    2. 8.2 Get Local Address
    3. 8.3 Set Baud Rate
    4. 8.4 Quit
  12. BR/EDR Commands
  13. 10GAPLE Commands
    1. 10.1  Set Discoverability Mode
    2. 10.2  Set Connectability Mode
    3. 10.3  Set Pairability Mode
    4. 10.4  Change Pairing Parameters
    5. 10.5  Advertise LE
    6. 10.6  Start Scanning
    7. 10.7  Stop Scanning
    8. 10.8  Connect LE
    9. 10.9  Disconnect LE
    10. 10.10 Pair LE
    11. 10.11 LE Pass Key Response
    12. 10.12 LE Query Encryption
    13. 10.13 Set Passkey
    14. 10.14 Discover GAPS
    15. 10.15 Get Local Name
    16. 10.16 Set Local Name
    17. 10.17 Get Remote Name
    18. 10.18 LE User Confirmation Response
    19. 10.19 Enable SC Only
    20. 10.20 Regenerate P256 Local Keys
    21. 10.21 SC Generate OOB Local Params
    22. 10.22 Set Local Appearance
    23. 10.23 Get Local Appearance
  14. 11SPPLE Commands
    1. 11.1 Discover SPPLE
    2. 11.2 Register SPPLE
    3. 11.3 LE Send
    4. 11.4 Configure SPPLE
    5. 11.5 LE Read
    6. 11.6 Loopback
    7. 11.7 Display Raw Mode Data
    8. 11.8 Automatic Read Mode
  15. 12References
  16. 13Revision History

Multiple SPPLE Connections Guide

Two SPPLE Connections

  1. In This version, we test two simultaneous SPPLE connections to the MSP430. The remote devices are used as a peripheral device while the MSP430 acts as the central device.
  2. Connect to the first device, discover and configure services on the first device. When discovering services and configuring services we have to specify the remote BD_ADDR that weconnected to.
  3. Similarly, Connect to the second device, discover and configure services on the second device.
  4. To send data to the first remote device data we use LeSend <BD-ADDR> <Number of Bytes to be sent>.

  5. To send data to the second remote device data we use LeSend <BD-ADDR> <Number of Bytes to be sent>.

  6. To read data from the first remote device data we use LeRead <BD-ADDR>.

  7. To read data from the second remote device data we use LeRead <BD-ADDR>.

  8. When the Automaticreadmode, DisplayRawmodedata or Loopback turns on, both connections turn on.

One SPP and One SPPLE Connection

  1. In this version, test an SPP connection and SPPLE Connection at the same time to the MSP430. One of the remote devices is used as a peripheral LE device while the remote deviceas SPP Client.
  2. Connect to the first device, discover and configure services on the first device. When discovering services and configuring services we have to specify the remote BD_ADDR that weconnected to.
  3. Open an SPP server and let the second remote device connect.
  4. To send data to the first remote device data we use LeSend <BD-ADDR> <Number of Bytes to be sent>.
  5. To send data to the second remote data we use CBSend <Number of Bytes to be sent> <Serial Port ID> . If we want to write a small amount of data we use the command Write <Serial Port ID>.
  6. To read data from the first remote device data we use LeRead <BD-ADDR>.
  7. To read data from the second remote device data we use Read.
  8. Turn on Automaticreadmode, DisplayRawmodedata or Loopback (turns on for both connections.)