DLPU126 December 2023 DLP470TE , DLP660TE , DLP780TE , DLPC4420
Before connecting the DLP660TEEVM, DLP470TEEVM or DLP780TEEVM to the DLPC4420AEVM, identify the male connector on the back of the DLP660TEEVM, DLP470TEEVM or DLP780TEEVM.
The connectors are keyed by design and must follow an orientation to mate with the female connector (J57) located on the DLPC4420AEVM.
The EVM looks like Figure 3-5 after the FMC cables have been properly connected between the DLP660TEEVM and the DLPC4420AEVM. The process is the same for use with the DLP470TEEVM and DLP780TEEVM.