SBOU113A June 2011 – January 2023
The Register tab contains information on the individual operation of the INA226 registers. Each register can be changed on a bit-by-bit basis to allow the user to have total control of the device beyond the general functionality of the GUI alone. Most of this functionality is displayed in the Configuration register tab, but if the user selects the appropriate register and clicks the Help With Reg button on the Register tab, as shown in Figure 6-11, the user can diagnose the individual uses of each bit in each register.