Transient currents can cause issues
such as voltage droop that may lead to unstable ADC operation. Therefore, it is
important to design power supplies to accommodate both average and transient current
demand. Review the benefits and challenges of three different power-supply
options:
- Low dropout regulators (LDOs). TI
recommends using LDOs to power precision ADCs. LDOs offer many benefits, such as
excellent noise performance; low voltage ripple; and a small, simple
implementation. The most important benefit of an LDO is its ability to reliably
maintain the output voltage during transients while also providing low quiescent
current. For more information on how to select the best LDO for any application,
see Related Website section below.
- Linear regulators. Linear
regulators with standard dropout voltages can also be a good option if selecting
an LDO is cost-prohibitive. Linear regulators can reliably maintain the output
voltage during transients while also providing low quiescent current similar to
LDOs. The challenge with linear regulators is that the dropout voltage is
significantly larger, which can require specific voltage rails just to power
these devices. Linear regulators also tend to come in larger packages because
they are less efficient and must dissipate more heat. Additional heat can raise
the temperature of a closed system, which can contribute to drift errors in
precision systems.
- Shunt regulators. One of the most
cost-effective power-supply options is a shunt regulator. The cost savings come
at the expense of the additional complexity required to design a reliable
power-supply circuit. As an example, a precision ADC requiring bipolar supply
operation might use the TLV431 – a low-voltage, adjustable
shunt regulator – to generate ±2.5-V rails. You can use the TLV431 for this purpose because it has a low VREF. However, one
challenge with this regulator is that it can supply only a limited amount of
current. The TLV431 data sheet also requires a cathode current of
≥1 mA. These two restrictions limit the output-current capabilities of the
standard setup shown in Figure 5 and Figure 6.
Figure 5 and Figure 6 show that both the cathode current and the current supplied to the ADC must flow
through resistor R1. This configuration limits the supply current to (VSUP – VREF) /
R1, resulting in two design challenges. First, current flowing continuously through
R1 consumes power even with no applied load. Attempting to reduce R1 to increase the
available supply current also proportionally increases the static power dissipation.
Second, the maximum current set by R1 generally cannot support the hundreds of
milliamperes of transient current that the ADC requires. An inability to provide the
necessary current causes the supply voltage to droop, and can lead to unstable ADC
operation.
Mitigate these issues by adding two
components to the circuit in Figure 5 and Figure 6. Figure 7 and Figure 8 show a modified shunt regulator circuit that includes a transistor and a bias
resistor, Rb.
The power-supply circuit in Figure 7 and Figure 8 can provide more current compared to the system in Figure 5 and Figure 6 because the transistor eliminates any resistance between the supply input (VSUP)
and output (VOUT). This new circuit can also maintain a cathode current of ≥1 mA by
installing Rb instead of relying on R1. Resistors R1 and R2 therefore are only
required to set the output voltage as per Equation 1.
Equation 1.
For more information on how to use a
voltage reference as a shunt regulator, see Related Website section below.