SNLA224A June 2014 – January 2024 DS90UB913A-Q1 , DS90UB954-Q1 , DS90UB960-Q1
RIN+ noise is the noise measured on the deserializer board at the input of the RIN+ pin. The RIN+ noise must be less than 10 mV peak-to-peak between 0 and 50 MHz to prevent degradation of the FPD-Link signal.
To accurately measure RIN+ noise in the system, the image sensor and all other load carrying devices on the serializer side must be actively drawing current. The forward channel and back channel transmissions generated by the connected serializer and deserializer must also be disabled to prevent interference in the noise measurements. To disable the forward channel and back channel transmissions, the PDB pin on the serializer and deserializer devices must be pulled to GND. The image sensor is expected to contribute to the RIN+ noise when actively capturing video data. Therefore if the image sensor is not enabled at the time of measurement, the results do not accurately represent the RIN+ noise of the system. An example of the RIN+ noise measurement procedure is listed in the following: