TIDUED6B august 2018 – april 2023
The wireless RF range was measured to be approximately 70 m in a typical office environment with a direct line of sight.
There are ways to increase this distance even further. Using a whip antenna with gain instead of the passive PCB antenna could offer improvements in the wireless RF range. Another option would be to increase the transmit power of the CC1352 device at the expense of increased supply current during the radio transmission intervals.