SNLS604F September 2020 – April 2025 DP83TG720S-Q1
PRODUCTION DATA
Sleep state can be exited either locally (pin/register-write) or by remote link-partner.
Local sleep exit for Master mode PHY by :
Local sleep exit for Slave mode PHY by :
Device can be made to exit the sleep mode by link-partner by either of the following :
Details of these procedures are in the following table :
| Method | Device Mode | Procedure | Required Link-partner Cabability |
|---|---|---|---|
| Using Send-S | Master |
Step 1 : Start IEEE defined Send-S pattern from link-partner for atleast 1.25ms. Step 2 : Put link-partner in the normal mode to start the link-up. Note : Link-partner with low VOD can limit the remote wake-up upto a maximum of 5m cable. |
Link-partner needs to have a mode to send Send-S
pattern on demand in Slave mode also. One possible way is : Step 1 : Put link-partner in master mode for atleast 1.25ms. Step 2 : Put link-partner in normal mode to start the link-up |
| Slave |
Step 1 : Start IEEE defined Send-S pattern from link-partner for atleast 1.25ms. Step 2 : Put link-partner in the normal mode to start the link-up. Note : Link-partner with low VOD can limit the remote wake-up upto a maximum of 5m cable. Note : To keep the slave mode DP83TG720 in sleep mode, link-partner can be put in managed mode (where device is not allowed to start link-up sequence). |
Any IEEE compliant link-partner works, as master mode link-partner is supposed to send Send-S signals to start the link-up | |
| Using Send-T | Master |
Step 1 : Enable Send-T pattern on link-partner for atleast 1.25ms. Step 2 : Put link-partner in the normal mode to start the link-up. |
Link-partner needs to have a mode to send Send-T
pattern on demand. Swing during Send-T mode at pins of link-partner must be greater than 0.92V for remote wake-up over 15m cable. Link-partner with lower VOD can limit the remote wake-up to 5m cable. DP83T720 as link-partner can do the required with following steps : Step 1 : Enable Send-T pattern on DP83TG720 link-partner : write reg[0x0405]=0x7400; reg[0x0509]=0x4007 and reg[0x0576]=0x0500 Step 2 : After 100ms disable send-T pattern on DP83TG720 link-partner : write reg[0x0405]=x5800; reg[0x0509]=0x4005 and reg[0x0576]=0x0000 |
| Slave |
Step 1 : Enable Send-T pattern on link-partner for atleast 1.25ms. Step 2 : Put link-partner in the normal mode to start the link-up. |
Link-partner needs to have a mode to send Send-T
pattern on demand. Swing during Send-T mode at pins of link-partner must be greater than 0.92V for remote wake-up over 15m cable. Link-partner with lower VOD can limit the remote wake-up to 5m cable. DP83T720 as link-partner can do the required with following steps : Step 1 : Enable Send-T pattern on DP83TG720 link-partner : write reg[0x0405]=0x7400; reg[0x0509]=0x4007 and reg[0x0576]=0x0500 Step 2 : After 100ms disable send-T pattern on DP83TG720 link-partner : write reg[0x0405]=x5800; reg[0x0509]=0x4005 and reg[0x0576]=0x0000 |