SBAS639C October 2017 – July 2018 DRV5055-Q1
PRODUCTION DATA.
The device produces a linear response when the output voltage is within the specified VL range. Outside this range, sensitivity is reduced and nonlinear. Figure 16 and Figure 17 graph the magnetic response.
Equation 2 calculates parameter BL, the minimum linear sensing range at 25°C taking into account the maximum quiescent voltage and sensitivity tolerances.
The parameter SLE defines linearity error as the difference in sensitivity between any two positive B values, and any two negative B values, while the output is within the VL range.
The parameter SSE defines symmetry error as the difference in sensitivity between any positive B value and the negative B value of the same magnitude, while the output voltage is within the VL range.