SLOS414K May 2003 – April 2022 LM2904-Q1 , LM2904B-Q1 , LM2904BA-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Determine the gain required by the inverting amplifier using Equation 1 and Equation 2:


Once the desired gain is determined, choose a value for RI or RF. Choosing a value in the kilohm range is desirable because the amplifier circuit uses currents in the milliampere range. This ensures the part does not draw too much current. This example uses 10 kΩ for RI which means 36 kΩ is used for RF. This was determined by Equation 3.