SNAS555D June 2000 – December 2016 LM2907-N , LM2917-N
PRODUCTION DATA.
| PIN | I/O | DESCRIPTION | |
|---|---|---|---|
| NAME | NO. | ||
| COL | 5 | I | The collector of the bipolar junction transistor |
| CP1 | 2 | O | A capacitor placed on this pin will be charged up to VCC/2 by a constant current source of 180 µA typical at the start of every positive half cycle. At the beginning of negative half cycles this capacitor is discharged the same amount at the same rate. |
| CP2/IN+ | 3 | I/O | See pins CP1 and IN+. On 8-pin devices (8-pin LM2907 and LM2917) these two nodes share a pin and are internally connected. |
| EMIT | 4 | O | The emitter of the bipolar junction transistor |
| GND | — | G | Ground |
| IN+ | — | I | The noninverting input to the high gain op amp |
| IN– | 7 | I | The inverting input to the high gain op amp |
| NC | — | — | No connect |
| TACH+ | 1 | I | Positive terminal for the input signal that leads to the noninverting terminal of the internal Schmitt-Trigger comparator. |
| TACH–/GND | 8 | I | Negative terminal for the input signal that leads to the noninverting terminal of the internal Schmitt-Trigger comparator. (NOTE: On 8-pin devices, LM2907 and LM2917, this pin is internally connected to ground and must be tied to ground externally to provide the reference voltage of the device). |
| V+ | 6 | I | Supply voltage |
| PIN | I/O | DESCRIPTION | |
|---|---|---|---|
| NAME | NO. | ||
| COL | 8 | I | The collector of the bipolar junction transistor |
| CP1 | 2 | O | A capacitor placed on this pin will be charged up to VCC/2 by a constant current source of 180 µA typical at the start of every positive half cycle. At the beginning of negative half cycles this capacitor is discharged the same amount at the same rate. |
| CP2 | 3 | O | The charge pump sources current out of this pin equal to the absolute value of the capacitor current on CP1. A resistor and capacitor in parallel connected to this pin filters the current pulses into the output voltage. |
| EMIT | 5 | O | The emitter of the bipolar junction transistor |
| GND | 12 | G | Ground |
| IN+ | 4 | I | The noninverting input to the high gain op amp |
| IN– | 10 | I | The inverting input to the high gain op amp |
| NC | 6, 7, 13, 14 | — | No connect |
| TACH+ | 1 | I | Positive terminal for the input signal that leads to the noninverting terminal of the internal Schmitt-Trigger comparator. |
| TACH– | 11 | I | Negative terminal for the input signal that leads to the noninverting terminal of the internal Schmitt-Trigger comparator. |
| V+ | 9 | I | Supply voltage |