SNAS849 December 2024 LMX2624-SP
ADVANCE INFORMATION
| MODE | DESCRIPTION | SOFTWARE SETTINGS |
|---|---|---|
| RESET | Registers are held in the reset state. This device does have a power on reset, but good practice is to also do a software reset if there is any possibility of noise on the programming lines, especially if there is sharing with other devices. Also realize that there are registers not disclosed in the data sheet that are reset as well. | RESET = 1 POWERDOWN = 0 |
| POWERDOWN | Device is powered down. | POWERDOWN = 1 or CAL Pin = Low |
| Pin-mode | Device settings are determined by pin states on CDIV. | Any one of the CDIV0, CDIV1, CDIV2 pins has value other than LOW |
| Normal operating mode | This is used with at least one output on as a frequency synthesizer and the device can be controlled through the SPI | All CDIV pins needs to be LOW |
| SYNC mode | This is used where part of the channel divider is in the feedback path to provide deterministic phase. | VCO_PHASE_SYNC = 1 |
| SYSREF mode | In this mode, RFoutB is used to generate pulses for SYSREF. | VCO_PHASE_SYNC =1, SYSREF_EN = 1 |