SNVSCP2A March 2025 – August 2025 LP5815
PRODUCTION DATA
The LP5815 supports autonomous animation control for each channel. With the animation engine the device can realize vivid lighting effects while releasing the loading of external controller.
As showed in Figure 7-4, the LP5815 has 4 independent configurable animation engine units, ENGINE0, ENGINE1, ENGINE2 and ENGINE3. Any one of the 4 engines can be selected by each output channel. There are 4 engine orders to construct one engine unit. For each engine order, one pattern unit can be selected to execute when the engine order is enabled. At the bottom layer, there are 4 independent configurable pattern units.