To achieve optimized performance with a
high-frequency amplifier such as the OPA810-Q1requires,
pay careful attention to board layout parasitics and external component types. The
DEM-OPA-SOT-1A can be used as a reference when
designing the circuit board. Recommendations that optimize performance include:
- Minimize parasitic capacitance to any ac
ground for all signal I/O pins. Parasitic capacitance on the output and
inverting input pins can cause instability—on the noninverting input, this
capacitance can react with the source impedance to cause unintentional
band-limiting. To reduce unwanted capacitance, open a window around the signal
I/O pins in all ground and power planes around those pins. Otherwise, ground and
power planes must be unbroken elsewhere on the board.
- Minimize the distance (< 0.1 inch) from
the power-supply pins to high-frequency, 0.01µF decoupling capacitors. At the
device pins, do not allow the ground and power plane layout to be in close
proximity to the signal I/O pins. Avoid narrow power and ground traces to
minimize inductance between the pins and the decoupling capacitors. Always
decouple the power-supply connections with these capacitors. Use larger (2.2µF
to 6.8µF) decoupling capacitors, effective at lower frequency, on the supply
pins. Place these capacitors somewhat farther from the device and share these
capacitors among several devices in the same area of the PCB.
- Careful selection and placement of external
components preserve the high-frequency performance of the OPA810-Q1.
Resistors must be a low reactance type. Surface-mount resistors work best and
allow a tighter overall layout. Metal film and carbon composition axially leaded
resistors can also provide good high-frequency performance. Again, keep the
leads and PCB trace length as short as possible. Never use wirewound type
resistors in a high-frequency application. Because the output pin and inverting
input pin are the most sensitive to parasitic capacitance, always position the
feedback and series output resistor, if any, as close as possible to the output
pin. Other network components, such as noninverting input termination resistors,
must also be placed close to the package. Even with a low parasitic capacitance
shunting the external resistors, excessively high resistor values can create
significant time constants that can degrade performance. Good axial metal film
or surface-mount resistors have approximately 0.2pF in shunt with the resistor.
For resistor values greater than 10kΩ, this parasitic capacitance can add a pole
or zero close to the GBWP of 70MHz and subsequently affects circuit operation.
Keep resistor values as low as possible and consistent with load driving
considerations. Lowering the resistor values keeps the resistor noise terms low,
and minimizes the effect of parasitic capacitance, however lower resistor values
increase the dynamic power consumption because RF and RG
become part of the amplifiers output load network. Transimpedance applications
(see also Section 8.2.1) can use whatever feedback resistor is required by the application as
long as the feedback compensation capacitor is set considering all parasitic
capacitance terms on the inverting node.
- Connections to other
wideband devices on the board can be made with short direct traces or
through on-board transmission lines. For short connections, consider the trace
and the input to the next device as a lumped capacitive load. Relatively wide
traces (50 mils to 100 mils) must be used, preferably with ground and power
planes opened up around them. Estimate the total capacitive load and set
RS for sufficient phase margin and stability. Low parasitic
capacitive loads (< 10pF) do not always require an RS because the
OPA810-Q1 is nominally compensated to operate
with a 10pF parasitic load. Higher parasitic capacitive loads without an
RS are allowed with increase in signal gain (increasing the
unloaded phase margin). If a long trace is required, and the 6dB signal loss
intrinsic to a doubly-terminated transmission line is acceptable, implement a
matched impedance transmission line using micro-strip or strip-line techniques
(consult an ECL design handbook for micro-strip and strip-line layout
techniques). A 50Ω environment is normally not necessary onboard, and a higher
impedance environment improves distortion. With a characteristic board trace
impedance defined based on board material and trace dimensions, a matching
series resistor into the trace from the output of the OPA810-Q1 is used as well as a terminating shunt resistor at the input
of the destination device. Remember also that the terminating impedance is the
parallel combination of the shunt resistor and the input impedance of the
destination device; set this total effective impedance to match the trace
impedance. If the 6dB attenuation of a doubly-terminated transmission line is
unacceptable, a long trace can be series-terminated at the source end only.
Treat the trace as a capacitive load in this case and set the series resistor
value to obtain sufficient phase margin and stability. This does not preserve
signal integrity as well as a doubly-terminated line. If the input impedance of
the destination device is low, the signal attenuates because of the voltage
divider formed by the series output into the terminating impedance.
- Take care to design the PCB layout for optimized
thermal dissipation. For the extreme case of 125°C operating ambient,
using the approximate 134.8°C/W for the SOIC package, and an internal power of
24V supply × 4.7mA 125°C supply current gives a maximum internal power
dissipation of 113mW. This power gives a 15°C increase from ambient to junction
temperature. Load power adds to this value, and this dissipation must also be
calculated to determine the worst-case safe operating point.
- Do not socket a high-speed device such as the
OPA810-Q1. The additional lead length
and pin-to-pin capacitance introduced by the socket can create an extremely
troublesome parasitic network that can almost make achieving a smooth, stable
frequency response impossible. Best results are obtained by soldering the OPA810-Q1 onto the board.