SBOS697B September 2014 – July 2026 REF19
PRODUCTION DATA
Low-side current sensing is desirable because the common-mode voltage is near ground. Therefore, the current-sensing design is independent of the bus voltage, VBUS. When sensing bidirectional currents, use a differential amplifier with a reference pin. This procedure allows for the differentiation between positive and negative currents by biasing the output stage such that it can respond to negative input voltages. There are a variety of methods for supplying power (V+) and the reference voltage (VREF, or VBIAS) to the differential amplifier. For a low-drift design, use a monolithic reference that supplies both power and the reference voltage. Figure 9-2 shows the general circuit topology for a low-drift, low-side, bidirectional, current-sensing design. This topology is particularly useful when interfacing with an ADC; see Figure 9-1. Not only do VREF and VBIAS track over temperature, but the matching is much better than alternate topologies. For a more detailed version of the design procedure, see the Low-Drift Bidirectional Single-Supply Low-Side Current Sensing Design Guide.
Figure 9-2 Low-Drift, Low-side, Bidirectional, Current-Sensing Circuit TopologyThe transfer function for the circuit given in Figure 9-2 is as shown in Equation 6: