SLPS785A December 2023 – October 2025 RES11A
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
This document uses the form
to describe the error of many of the RES11A parameters in a ratiometric manner. This expression expands to
Thus, the difference or absolute error between the actual and nominal value of a given parameter is
Paramactual shares the same units as Paramnominal, such as V/V or Ω/Ω when describing circuit gain, while tParam is unitless by default. Because the error tolerances of the RES11A are so low, tParam errors are typically expressed in units of ppm, by multiplying the error by 106. To convert tParam from ppm back to a unitless decimal value for error calculations, divide the tValue by 106. Refer to Section 7.3.1 for an example of this.
As many of the RES11A error terms (such as gain error and gain temperature coefficients) scale according to the nominal gain, this notation provides a convenient way to standardize values across the various RES11A ratios. When converting ratiometric errors to absolute errors (or vice versa) for error analysis calculations, be cautious of notation and remember to scale tParam errors by Paramnominal when appropriate. Section 9.7 includes a list of the various error terms that appear throughout the document, and a summary or definition of each.
In some cases, such as when describing divider ratio or gain, the same equation applies to both divider 1 and divider 2. In this case, a notation of Paramx is used, where x is either 1 or 2. For example, when generically describing ratio error,
For the ratio error of divider 2 specifically,