SCDS488 December 2025 TMUX2819 , TMUX2821
PRODUCTION DATA
Bandwidth is defined as the range of frequencies that are attenuated by less than 3dB when the input is applied to the source pin (Sx) of an on-channel, and the output is measured at the drain pin (Dx) of the device. Figure 6-12 shows the setup used to measure bandwidth.