SLVSIF2 July 2025 TPD4S201
PRODUCTION DATA
USB PD has a specification for the total amount of capacitance that is required for proper USB PD BMC operation on the CC lines.
| NAME | DESCRIPTION | MIN | MAX | UNIT | COMMENT |
|---|---|---|---|---|---|
| cReceiver | CC receiver capacitance | 200 | 600 | pF | The DFP or UFP system have capacitance within this range when not transmitting on the line |
When USB PD is in use, keep the capacitance of the CC lines between 200pF and 600pF. The combination of capacitances added to the system by the TPS25751, the TPD4S201, and any external capacitor need to fall within these limits.