SLVSB97E July 2012 – January 2018 TPS23751 , TPS23752
PRODUCTION DATA.
The TPS23751 and TPS23752 have a number of internal comparators with hysteresis for stable switching between the various states. Figure 23 relates the parameters in the Electrical Characteristics section to the PoE states. The mode labeled Idle between Classification and Operation implies that the DEN, CLS, and RTN pins are all high impedance. The state labeled Mark, which is drawn in dashed lines, is part of the new type 2 hardware class state machine.

NOTE:
Variable names refer to Electrical Characteristic table parameters