SGLS228C December 2003 – September 2015 TPS3805H33-Q1
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
The TPS380x-Q1 devices are low-current supervisory circuits used to monitor system voltages above 1.226 V. The devices assert an active low RESET signal when VDD ,SENSE, or both voltages drop below a preset threshold. The RESET output remains low until the VDD, SENSE, or both voltages return above their thresholds. The devices are also designed to be immune to short negative transients on the VDD and SENSE pins.
The VDD and SENSE inputs provide a pin at which a system voltage can be monitored. If the voltage on this pin drops below VIT, RESET is asserted low. The comparator has a built-in hysteresis to ensure smooth RESET assertions and de-assertions. Refer to the Device Comparison Table to determine the VDD and SENSE voltage thresholds for each device. The adjustable version TPS3803-01-Q1 can be used to monitor any voltage rail down to 1.226 V using the circuit shown in Figure 13, where VIT' is the Vin threshold voltage.
Figure 13. Using Adjustable Version
The TPS380x-Q1 devices are immune to short negative transients on the VDD and SENSE pins. Sensitivity to transients is dependent on threshold overdrive as shown in Figure 15 and Figure 16. These graphs show the duration that the transient is below VIT compared to the magnitude of the voltage drop below VIT, called the threshold overdrive voltage. Any combination of transient duration and overdrive voltage which lies above the curves will result in RESET being asserted low. Any transient which lies below the curves will be ignored by the device.
Figure 14. Overdrive Voltage
TPS3803-01-Q1 and TPS3803G15-Q1 monitor only one supply, which is SENSE and VDD respectively. When that supply is above the VIT threshold, RESET will be high. Otherwise, RESET will be low. TPS3805H33-Q1 monitors both VDD and SENSE. When both VDD and SENSE are above the VIT threshold, RESET will be high. Otherwise, RESET will be low.
| TPS3803-01-Q1 | |
|---|---|
| SENSE > VIT | RESET |
| 0 | L |
| 1 | H |
| TPS3803G15-Q1 | |
|---|---|
| VDD > VIT | RESET |
| 0 | L |
| 1 | H |
| TPS3805H33-Q1 | ||
|---|---|---|
| VDD > VIT | SENSE > VIT | RESET |
| 0 | 0 | L |
| 0 | 1 | L |
| 1 | 0 | L |
| 1 | 1 | H |