SLVSEW8B August 2019 – December 2019 TPS66020 , TPS66021
PRODUCTION DATA.
The timing diagram of enabling the PP5V Source path with a current limit set to 1.5 A is shown in Figure 20. As shown, transitions from either the Source path to the Sink path or vice-versa always requires a transition first to the DISABLED state, EN1_EN0 = 00b. Figure 21 shows the timing diagram going from a Sink to a 3-A Source. Figure 22 shows changing the current limit back to 1.5 A from its original 3-A setting.
Figure 20. Enabling the PP5V Source Path to 1.5-A Current Limit
Figure 21. Enabling the PP5V Source Path to 3-A Current Limit
Figure 22. Changing the PP5V Source Path from 3-A to 1.5-A Current Limit