SLUSD31F October 2018 – July 2026 UCC23513
PRODUCTION DATA
The total loss, PG, in the gate-driver subsystem includes the power losses (PGD) of the UCC23513 device and the power losses in the peripheral circuitry, such as the external gate-drive resistor.
The PGD value is the key power loss which determines the thermal safety-related limits of the UCC23513 device. Estimate the PGD value by calculating losses from several components.
The first component is the static power loss, PGDQ, which includes power dissipated in the input stage (PGDQ_IN) as well as the quiescent power dissipated in the output stage (PGDQ_OUT) when operating with a certain switching frequency under no load. Determine PGDQ_IN by IF and VF and is given by Equation 5. The PGDQ_OUT parameter is measured on the bench with no load connected to VOUT pin at a given VCC, switching frequency, and ambient temperature. In this example, VCC is 15V. The measurement of current on the power supply, with PWM switching at 10kHz, is ICC = 1.33mA. Therefore, use Equation 6 to calculate PGDQ_OUT.
The total quiescent power (without any load capacitance) dissipated in the gate driver is the sum of Equation 5 and Equation 6 as Equation 7 shows.
The second component is the switching operation loss, PGDSW, with a given load capacitance which the driver charges and discharges the load during each switching cycle. Use Equation 8 to calculate the total dynamic loss from load switching, PGSW.
where
So, for this example application the total dynamic loss from load switching is approximately 18mW as calculated in Equation 9.
QG represents the total gate charge of the power transistor switching 520V at 50A, and is subject to change with different testing conditions. The UCC23513 gate-driver loss on the output stage, PGDO, is part of PGSW. PGDO is equal to PGSW if the external gate-driver resistance and power-transistor internal resistance are 0Ω, and all the gate driver-loss dissipates inside the UCC23513. If an external turn-on and turn-off resistance exists, the total loss is distributed between the gate driver pull-up and pull-down resistance, external gate resistance, and power-transistor internal resistance. Importantly, the pull-up and pull-down resistance is a linear and fixed resistance if the source/sink current is not saturated to 4.5A/5.3A, however, it is nonlinear if the source/sink current is saturated. Therefore, PGDO is different in these two scenarios.