JAJSGA0A September 2018 – August 2019 ADS1284
PRODUCTION DATA.
Read-data-continuous mode is stopped by the SDATAC command and then places the ADC into read-data-by-command mode. In read-data-by-command mode, an RDATA command is sent to the device in order to read each new conversion data (as shown in Figure 62). When the read data command is received (on the eighth SCLK rising edge), data are available to read only when DRDY subsequently goes low (tDR). When DRDY goes low, conversion data appear on DOUT. The data may be read on the rising edge of SCLK.
| PARAMETER | MIN | TYP | MAX | UNIT | |
|---|---|---|---|---|---|
| tDR | Time for new data after data read command | 0 | 1 | fDATA | |