JAJSP46A May 2023 – September 2023 AMC130M03
PRODUCTION DATA
Multiple registers are read from the device when nnn nnnn is specified as a number greater than zero in the RREG command word. As with all SPI commands on the AMC130M03, the response occurs on the output in the frame following the command. Instead of a single acknowledgment word, the response spans multiple words to shift out all requested registers. Continue toggling SCLK to accommodate outputting the entire data stream. ADC conversion data are not output in the frame following an RREG command to read multiple registers. Figure 8-28 shows an example of reading multiple registers.