JAJSFD3G August   2016  – March 2019 DRA780 , DRA781 , DRA782 , DRA783 , DRA785 , DRA786 , DRA787 , DRA788
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
  • ABF|367
サーマルパッド・メカニカル・データ

On-Chip Debug

Debugging a system that contains an embedded processor involves an environment that connects high-level debugging software running on a host computer to a low-level debug interface supported by the target device. Between these levels, a debug and trace controller (DTC) facilitates communication between the host debugger and the debug support logic on the target chip.

The DTC is a combination of hardware and software that connects the host debugger to the target system. The DTC uses one or more hardware interfaces and/or protocols to convert actions dictated by the debugger user to JTAG® commands and scans that execute the core hardware.

The debug software and hardware components let the user control multiple central processing unit (CPU) cores embedded in the device in a global or local manner. This environment provides:

  • Synchronized global starting and stopping of multiple processors
  • Starting and stopping of an individual processor
  • Each processor can generate triggers that can be used to alter the execution flow of other processors

System topics include but are not limited to:

  • System clocking and power-down issues
  • Interconnection of multiple devices
  • Trigger channels

The device deploys Texas Instrument's CTools debug technology for on-chip debug and trace support. It provides the following features:

  • External debug interfaces:
    • Primary debug interface - IEEE1149.1 (JTAG) or IEEE1149.7 (complementary superset of JTAG)
      • Used for debugger connection
      • Default mode is IEEE1149.1 but debugger can switch to IEEE1149.7 via an IEEE1149.7 adapter module
      • Controls ICEPick™ (generic test access port [TAP] for dynamic TAP insertion) to allow the debugger to access several debug resources through its secondary (output) JTAG ports (for more information, see section ICEPick Secondary TAPs in chapter On-Chip Debug Support of the Device TRM).
    • Debug (trace) port
      • Can be used to export processor or system trace off-chip (to an external trace receiver)
      • Can be used for cross-triggering with an external device
      • Configured through debug resources manager (DRM) module instantiated in the debug subsystem
      • For more information about debug (trace) port, see sections Debug (Trace) Port and Concurrent Debug Modes in chapter On-Chip Debug Support of the Device TRM.
  • JTAG based processor debug on:
    • C66x in DSP1, DSP2
    • Cortex-M4 (x2) in IPU
  • Dynamic TAP insertion
    • Controlled by ICEPick
    • For more information, see section Dynamic TAP Insertion in chapter On-Chip Debug Support of the Device TRM
  • Power and clock management
    • Debugger can get the status of the power domain associated to each TAP.
    • Debugger may prevent the application software switching off the power domain.
    • Application power management behavior can be preserved during debug across power transitions.
    • For more information, see section Power and Clock Management in chapter On-Chip Debug Support of the Device TRM.
  • Reset management
    • Debugger can configure ICEPick to assert, block, or extend the reset of a given subsystem.
    • For more information, see section Reset Management in chapter On-Chip Debug Support of the Device TRM.
  • Cross-triggering
    • Provides a way to propagate debug (trigger) events from one processor, subsystem, or module to another:
      • Subsystem A can be programmed to generate a debug event, which can then be exported as a global trigger across the device.
      • Subsystem B can be programmed to be sensitive to the trigger line input and to generate an action on trigger detection.
    • Two global trigger lines are implemented
    • Device-level cross-triggering is handled by the XTRIG (TI cross-trigger) module implemented in the debug subsystem
    • For more information about cross-triggering, see section Cross-Triggering in chapter On-Chip Debug Support of the Device TRM.
  • Suspend
    • Provides a way to stop a closely coupled hardware process running on a peripheral module when the host processor enters debug state
    • For more information about suspend, see section Suspend in chapter On-Chip Debug Support of the Device TRM.
  • Processor trace
    • C66x (DSP) processor trace is supported
    • Two exclusive trace sinks:
      • CoreSight Trace Port Interface Unit (CS_TPIU) – trace export to an external trace receiver
    • For more information, see section Processor Trace in chapter On-Chip Debug Support of the Device TRM.
  • System instrumentation (trace)
    • Supported by a CTools System Trace Module (CT_STM), implementing MIPI System Trace Protocol (STP) (rev 2.0)
    • Real-time software trace
      • System-on-chip (SoC) software instrumentation through CT_STM (STP2.0)
    • OCP watchpoint (OCP_WP_NOC)
      • OCP target traffic monitoring: OCP_WP_NOC can be configured to generate a trigger upon watchpoint match (that is, when target transaction attributes match the user-defined attributes).
      • SoC events trace
      • DMA transfer profiling
    • Statistics collector (performance probes)
      • Computes traffic statistics within a user-defined window and periodically reports to the user through the CT_STM interface
      • Embedded in the L3_MAIN interconnect
      • 10 instances:
        • 1 instance dedicated to target (SDRAM) load monitoring
        • 9 instances dedicated to master latency monitoring
    • Power-management events profiling (PM instrumentation [PMI])
      • Monitoring major power-management events. The PM state changes are handled as generic events and encapsulated in STP messages.
    • Clock-management events profiling CM instrumentation [CMI]) for CM_CORE_AON clocks
      • Monitoring major clock management events. The CM state changes are handled as generic events and encapsulated in STP messages.
      • One instances
        • CM1 Instrumentation (CMI1) module mapped in the PD_CORE_AON power domain
    • For more information, see section System Instrumentation in chapter On-Chip Debug Support of the Device TRM.
  • Performance monitoring
    • Supported by subsystem counter timer module (SCTM) for IPU

For more information, see chapter On-Chip Debug Support of the device TRM.