JAJSLD8B July 2021 – November 2021 INA823
PRODUCTION DATA
Figure 8-2 shows that the gain of the INA823 is set by a single external resistor (RG) connected between the RG pins (pins 1 and 8).
The gain of the INA823 can be calculated with Equation 1:
The value of the external gain resistor RG is then derived from the gain equation:
Table 8-1 lists several commonly used gains and resistor values. The 100-kΩ term in Equation 1 is a result of the sum of the two internal 50-kΩ feedback resistors. These on-chip resistors are laser-trimmed to accurate absolute values. The accuracy and temperature coefficients of these resistors are included in the gain accuracy and drift specifications of the Section 7.5. As shown in Figure 8-2 and explained in more details in Section 11, make sure to connect low-ESR, 0.1-µF ceramic bypass capacitors between each supply pin and ground that are placed as close to the device as possible.
DESIRED GAIN | NEAREST 1% RG (Ω) | CALCULATED GAIN ERROR (%) |
---|---|---|
1 | Not connected | Not connected |
2 | 100 k | 0 |
5 | 24.9 k | 0.321 |
10 | 11 k | 0.909 |
20 | 5.23 k | 0.602 |
33 | 3.09 k | 1.098 |
50 | 2.05 k | 0.439 |
65 | 1.58 k | 1.091 |
100 | 1.02 k | 0.961 |
200 | 499 | 0.700 |
500 | 200 | 0.200 |
1000 | 100 | 0.100 |