The minimum requirements for a suitable low dropout regulator are:
- The current drive capability must slightly exceed
the specified load current of the application to prevent the LDO from dropping out of
regulation. Therefore, for a load current of 550mA, choose a 600mA to 700mA LDO. While
regulators with higher drive capabilities are acceptable, these regulators also typically
possess higher dropout voltages that reduce the overall converter efficiency.
- The internal dropout voltage, VDO, at
the specified load current must be as low as possible to maintain efficiency. For a
low-cost 700mA LDO, a VDO of 600mV at 700mA is common. Be aware; however, that
this lower value is typically specified at room temperature and can increase by a factor
of 2 over temperature, which in turn raises the required minimum input voltage.
- The required minimum input voltage preventing the
regulator from dropping out of line regulation is given with:
Equation 1. VI-min = VDO-max +
VO-max
To
determine VI for worst-case condition, the user must take the maximum values
for VDO and VO specified in the LDO data sheet for rated output
current (that is, 600mA) and add these values together. The user must also specify that
the output voltage of the push-pull rectifier at the specified load current is equal or
higher than VI-min. If the output voltage is not, the LDO loses
line-regulation and any variations at the input passes straight through to the output.
Hence, below VI-min the output voltage follows the input and the regulator
behaves like a simple conductor.
- The maximum regulator input voltage must be
higher than the rectifier output under no-load. Under this condition there is no secondary
current reflected back to the primary, thus making the voltage drop across
RDS-on negligible and allowing the entire converter input voltage to drop
across the primary. At this point, the secondary reaches the maximum voltage of
Equation 2. VS-max =
VIN-max × n
with VIN-max as the maximum converter
input voltage and n as the transformer turns ratio. Thus to prevent the LDO from damage the
maximum regulator input voltage must be higher than VS-max. Table 7-3 lists the maximum
secondary voltages for various turns ratios commonly applied in push-pull converters.
Table 7-3 Required Maximum LDO Input Voltages for Various Push-Pull ConfigurationsPUSH-PULL CONVERTER | LDO |
---|
CONFIGURATION | VIN-max [V] | TURNS-RATIO | VS-max [V] | VI-max [V] |
---|
3.3VIN to 3.3VOUT | 3.6 | 1.5 ± 3% | 5.6 | 6 to 10 |
3.3VIN to 5VOUT | 3.6 | 2.2 ± 3% | 8.2 | 10 |
5VIN to 5VOUT | 5.5 | 1.5 ± 3% | 8.5 | 10 |