JAJSQR3A August 2023 – November 2023 LM5185-Q1
PRODUCTION DATA
Choose compensation components for a stable control loop using the procedure outlined as follows.
First, calculate the power stage transfer function with Equation 26. Lmag is the magnetizing inductance of the transformer. Cout is the output capacitance. Rload is the load resistance.
where
Next, use Equation 32 to calculate the power stage gain at the cross-over frequency Fco which is selected to be 1 kHz for this design.
Select RCOMP to satisfy the desired cross-over frequency.
Select CCOMP to set the compensator zero at 2 times of the load pole.
Select CHF to set the compensator pole at 50 to 200 times the compensator zero.