JAJSFJ6C October 2012 – May 2018 TMS570LS0332 , TMS570LS0432
PRODUCTION DATA.
| EVENT NUMBER | SOURCE SELECT BITS
For G1, G2, or EVENT (G1SRC[2:0], G2SRC[2:0], or EVSRC[2:0]) |
TRIGGER |
|---|---|---|
| 1 | 000 | ADEVT |
| 2 | 001 | N2HET[8] |
| 3 | 010 | N2HET[10] |
| 4 | 011 | RTI compare 0 interrupt |
| 5 | 100 | N2HET[12] |
| 6 | 101 | N2HET[14] |
| 7 | 110 | N2HET[17] |
| 8 | 111 | N2HET[19] |
NOTE
For ADEVT, N2HET trigger sources, the connection to the MibADC module trigger input is made from the output side of the input buffer. This way, a trigger condition can be generated either by configuring the function as output onto the pad, or by driving the function from an external trigger source as input. If the mux controller module is used to select different functionality instead of ADEVT or N2HET[x], care must be taken to disable these signals from triggering conversions; there is no multiplexing on input connections.
NOTE
For the RTI compare 0 interrupt source, the connection is made directly from the output of the RTI module. That is, the interrupt condition can be used as a trigger source even if the actual interrupt is not signaled to the CPU.