JAJSE28B October 2017 – August 2018 UCC27710
PRODUCTION DATA.
The power losses of UCC27710 (PUCC27710) are estimated by calculating losses from several components. The gate drive loss in the UCC27710 is typically dominated by gate drive losses associated with charging and discharging the power device gate charge. There are other losses to consider outlined below.
To determine the UCC27710 operating with no driver load, refer to the Typical Characteristics Figure 26 for IDD and IHB to determine the operating current at the appropriate fSW. The operating current power losses with no driver load are calculated in Equation 15:
Static losses due to leakage current (IBL) are calculated from the HB high-voltage node as shown in Equation 16:
Equation 17 calculates dynamic losses during the operation of the level shifter at HO turn-off edge. QP, typically 0.6 nC, is the charge absorbed by the level shifter during operation at each edge. Please note that if high-voltage switching occurs during HO turn-on as well (as in the case of ZVS topologies), then the power loss due to this component must be effectively doubled.
where
Dynamic losses incurred due to the gate charge while driving the FETs Q1 and Q2 are calculated Equation 18. Please note that this component typically dominates over the dynamic losses related to the internal VDD and VHB switching logic circuitry in UCC27710. The losses incurred driving the gate charge are not all dissipated in the gate driver device, this includes losses in the external gate resistance and internal power switch gate resistance.
The UCC27710 gate driver loss on the output stage ,PGDO, is part of PQG1,QG2. If the external gate resistances are zero most of the PQG1,QG2 will be dissipated in the UCC27710. If there are external gate resistances, the total loss will be distributed between the gate driver pull-up/down resistances and the external gate resistances.
The gate drive power dissipated within the UCC27710 driver can be determined by Equation 19:
In this example the gate drive related losses are approximately 24 mW as shown in Equation 19:
For the conditions, VDD=12 V, VHB = 400 V, HO On-state Duty cycle D = 50%, QG = 31 nC, fSW = 100 kHz, the total power loss in UCC27710 driver for a half bridge power supply topology can be estimated as follows: