DLPU132B October 2023 – March 2025
The Start Page is the first window that users see upon executing the DLPC964 GUI.
This window has the image of a standard setup for the Apps FPGA (AMD EVM) with DLPLCRC964EVM and DLPLCR99EVM / DLPLCR99UVEVM.
There are also online resources to help enable customers to get Evaluation Module Kits started.
Figure 3-4 DLPC964 GUI Start WindowIf the DLPC964 GUI states that Hardware is not connected, then check: