DLPU132B October 2023 – March 2025
The DLPC964 Registers tab uses the I2C Interface to communicate with the DLPC964 controller registers. This tab shows the DLPC964 controller register list and settings for each register which use Get/Set buttons to read/write to specific registers.
Figure 3-11 DLPC964 Register ListRegister Definitions
The following designations are used throughout this section of the document:
Please visit the DLPC964 data sheet for detailed descriptions of each DLPC964 register offered in the DLPC964 GUI.