JAJS168H June 2005 – June 2025 ADS1232 , ADS1234
PRODUCTION DATA
The voltage reference used by the modulator is generated from the voltage difference between pins REFP and REFN: VREF = V(REFP) – V(REFN). The reference inputs use a structure similar to that of the analog inputs. In order to increase the reference input impedance, a switching buffer circuitry is used to reduce the input equivalent capacitance. The reference drift and noise impact ADC performance. In order to achieve best results, pay close attention to the reference noise and drift specifications. A simplified diagram of the circuitry on the reference inputs is shown in Figure 7-3. The switches and capacitors can be modeled with an effective impedance of:

where
For the ADS123x:
Figure 7-3 Simplified Reference Input CircuitryESD diodes protect the reference inputs. To prevent these diodes from turning on, make sure the voltages on the reference pins do not go below AGND by more than 100 mV; and likewise, do not exceed AVDD by 100 mV:
AGND – 100 mV < V(REFP) or V(REFN) < AVDD + 100 mV