JAJSE94B december 2017 – august 2023 LMK61E07
PRODUCTION DATA
The NVMDAT register returns the on-chip EEPROM contents from the starting address specified by the MEMADR register.
BIT NO. | FIELD | TYPE | DEFAULT | EEPROM | DESCRIPTION |
---|---|---|---|---|---|
[7:0] | NVMDAT[7:0] | R | 0x00 | N | EEPROM Read Data. The first time an I2C read transaction
accesses the NVMDAT register address, either because it was explicitly targeted or
because the address was auto-incremented, the read transaction will return the
EEPROM data located at the address specified by the MEMADR register. Any additional
reads which are part of the same transaction will cause the EEPROM address to be
incremented and the next EEPROM data byte will be returned. The I2C
address will no longer be auto-incremented, that is the I2C address will
be locked to the NVMDAT register after the first access. Access to the NVMDAT
register will terminate at the end of the current I2C
transaction. |