JAJSE94B december 2017 – august 2023 LMK61E07
PRODUCTION DATA
The NVMCTL register allows control of the on-chip EEPROM Memories.
| BIT NO. | FIELD | TYPE | DEFAULT | EEPROM | DESCRIPTION |
|---|---|---|---|---|---|
| [7] | RESERVED | - | - | N |
Reserved. |
| [6] | REGCOMMIT | RWSC | 0 | N |
REG Commit to EEPROM SRAM Array.
The REGCOMMIT bit is used to initiate a transfer from the on-chip registers back to the corresponding location in the EEPROM SRAM Array. The REGCOMMIT bit is automatically cleared to 0 when the transfer is complete. |
| [5] | NVMCRCERR | R | 0 | N |
EEPROM CRC Error Indication.
The NVMCRCERR bit is set to 1 if a CRC Error has been detected when reading back from on-chip EEPROM during device configuration. |
| [4] | NVMAUTOCRC | RW | 1 | N |
EEPROM Automatic CRC.
When NVMAUTOCRC is 1 then the EEPROM Stored CRC byte is automatically calculated whenever a EEPROM program takes place. |
| [3] | NVMCOMMIT | RWSC | 0 | N |
EEPROM Commit to Registers.
The NVMCOMMIT bit is used to initiate a transfer of the on-chip EEPROM contents to internal registers. The transfer happens automatically after reset or when NVMCOMMIT is set to 1. The NVMCOMMIT bit is automatically cleared to 0. The I2C registers cannot be read while a EEPROM Commit operation is taking place. |
| [2] | NVMBUSY | R | 0 | N |
EEPROM Program Busy Indication.
The NVMBUSY bit is 1 during an on-chip EEPROM Erase/Program cycle. While NVMBUSY is 1 the on-chip EEPROM cannot be accessed. |
| [1] | NVMERASE | RWSC | 0 | N |
EEPROM Erase Start.
The NVMERASE bit is used to begin an on-chip EEPROM Erase cycle. The Erase cycle is only initiated if the immediately preceding I2C transaction was a write to the NVMUNLK register with the appropriate code. The NVMERASE bit is automatically cleared to 0. The EEPROM Erase operation takes around 115ms. |
| [0] | NVMPROG | RWSC | 0 | N |
EEPROM Program Start.
The NVMPROG bit is used to begin an on-chip EEPROM Program cycle. The Program cycle is only initiated if the immediately preceding I2C transaction was a write to the NVMUNLK register with the appropriate code. The NVMPROG bit is automatically cleared to 0. If the NVMERASE and NVMPROG bits are set simultaneously then an ERASE/PROGRAM cycle will be executed The EEPROM Program operation takes around 115ms. |