JAJSGO9C July 2013 – May 2017 TAS5760L
PRODUCTION DATA.
| TAS5760L | NO. | TYPE(1) | INTERNAL TERMINATION | DESCRIPTION |
|---|---|---|---|---|
| NAME | ||||
| AVDD | 46 | P | - | Power supply for internal analog circuitry |
| ANA_REF | 4 | P | - | Connection point for internal reference used by ANA_REG and VCOM filter capacitors |
| ANA_REG | 2 | P | - | Voltage regulator derived from AVDD supply (NOTE: This terminal is provided as a connection point for filtering capacitors for this supply and must not be used to power any external circuitry) |
| BSTRPA- | 39 | P | - | Connection point for the SPK_OUTA- bootstrap capacitor, which is used to create a power supply for the high-side gate drive for SPK_OUTA- |
| BSTRPA+ | 43 | P | - | Connection point for the SPK_OUTA+ bootstrap capacitor, which is used to create a power supply for the high-side gate drive for SPK_OUTA |
| BSTRPB- | 38 | P | - | Connection point for the SPK_OUTB- bootstrap capacitor, which is used to create a power supply for the high-side gate drive for SPK_OUTB- |
| BSTRPB+ | 34 | P | - | Connection point for the SPK_OUTB+ bootstrap capacitor, which is used to create a power supply for the high-side gate drive for SPK_OUTB+ |
| DGND | 17 | G | - | Ground for digital circuitry (NOTE: This pin should be connected to the system ground) |
| DVDD | 9 | P | - | Power supply for the internal digital circuitry |
| FREQ/SDA | 7 | DI | Weak Pull-Down | Dual function pin that functions as an I²C data input pin in I²C Control Mode or as a Frequency Select terminal when in Hardware Control Mode. |
| GGND | 47 | G | - | Ground for gate drive circuitry (this terminal should be connected to the system ground) |
| GVDD_REG | 48 | P | - | Voltage regulator derived from PVDD supply (NOTE: This pin is provided as a connection point for filtering capacitors for this supply and must not be used to power any external circuitry) |
| LRCK | 16 | DI | Weak Pull-Down | Word select clock for the digital signal that is active on the serial port's input data line |
| MCLK | 13 | DI | Weak Pull-Down | Master Clock used for internal clock tree, sub-circuit/state machine, and Serial Audio Port clocking |
| NC | 18-31 | - | - | Not connected inside the device (all "no connect" pins should be connected to ground for best thermal performance, however they can be used as routing channels if required.) |
| PBTL/SCL | 8 | DI | Weak Pull-Down | Dual function pin that functions as an I²C clock input terminal in I²C Control Mode or configures the device to operate in pre-filter Parallel Bridge Tied Load (PBTL) mode when in Hardware Control Mode |
| PGND | 36, 41 | G | - | Ground for power device circuitry (NOTE: This terminal should be connected to the system ground) |
| PVDD | 32, 33, 44, 45 | P | - | Power Supply for internal power circuitry |
| SCLK | 14 | DI | Weak Pull-Down | Bit clock for the digital signal that is active on the serial data port's input data line |
| SDIN | 15 | DI | Weak Pull-Down | Data line to the serial data port |
| SFT_CLIP | 1 | AI | - | sets the maximum output voltage before clipping |
| SPK_FAULT | 5 | DO | - | Speaker amplifier fault terminal, which is pulled LOW when an internal fault occurs |
| SPK_GAIN0 | 10 | DI | Weak Pull-Down | Adjusts the LSB of the multi-bit gain of the speaker amplifier |
| SPK_GAIN1 | 11 | DI | Weak Pull-Down | Adjusts the MSB of the multi-bit gain of the speaker amplifier |
| SPK_SLEEP/ADR | 12 | DI | Weak Pull-Up | In Hardware Control Mode, places the speaker amplifier in sleep mode. In Software Control Mode, is used to determine the I²C Address of the device |
| SPK_OUTA- | 40 | AO | - | Negative pin for differential speaker amplifier output A |
| SPK_OUTA+ | 42 | AO | - | Positive pin for differential speaker amplifier output A |
| SPK_OUTB- | 37 | AO | - | Negative pin for differential speaker amplifier output B |
| SPK_OUTB+ | 35 | AO | - | Positive pin for differential speaker amplifier output B |
| SPK_SD | 6 | AO | - | Places the speaker amplifier in shutdown |
| VCOM | 3 | P | - | Bias voltage for internal PWM conversion block |
| PowerPAD™ | - | G | - | Provides both electrical and thermal connection from the device to the board. A matching ground pad must be provided on the PCB and the device connected to it via solder. For proper electrical operation, this ground pad must be connected to the system ground. |
| TAS5760L | NO. | TYPE(1) | INTERNAL TERMINATION | DESCRIPTION |
|---|---|---|---|---|
| NAME | ||||
| AVDD | 1 | P | - | Power supply for internal analog circuitry |
| ANA_REF | 5 | P | - | Connection point for internal reference used by ANA_REG and VCOM filter capacitors |
| ANA_REG | 3 | P | - | Voltage regulator derived from AVDD supply (NOTE: This terminal is provided as a connection point for filtering capacitors for this supply and must not be used to power any external circuitry) |
| BSTRPA– | 25 | P | - | Connection point for the SPK_OUTA– bootstrap capacitor, which is used to create a power supply for the high-side gate drive for SPK_OUTA– |
| BSTRPA+ | 30 | P | - | Connection point for the SPK_OUTA+ bootstrap capacitor, which is used to create a power supply for the high-side gate drive for SPK_OUTA |
| BSTRPB– | 24 | P | - | Connection point for the SPK_OUT bootstrap capacitor, which is used to create a power supply for the high-side gate drive for SPK_OUT |
| BSTRPB+ | 19 | P | - | Connection point for the SPK_OUTB+ bootstrap capacitor, which is used to create a power supply for the high-side gate drive for SPK_OUTB+ |
| DGND | 18 | G | - | Ground for digital circuitry (NOTE: This terminal should be connected to the system ground) |
| DVDD | 10 | P | - | Power supply for the internal digital circuitry |
| FREQ/SDA | 8 | DI | Weak Pull-Down | Dual function terminal that functions as an I²C data input terminal in I²C Control Mode or as a Frequency Select terminal when in Hardware Control Mode. |
| GGND | 31 | G | - | Ground for gate drive circuitry (this terminal should be connected to the system ground) |
| GVDD_REG | 32 | P | - | Voltage regulator derived from PVDD supply (NOTE: This terminal is provided as a connection point for filtering capacitors for this supply and must not be used to power any external circuitry) |
| LRCK | 17 | DI | Weak Pull-Down | Word select clock for the digital signal that is active on the serial port's input data line |
| MCLK | 14 | DI | Weak Pull-Down | Master Clock used for internal clock tree, sub-circuit/state machine, and Serial Audio Port clocking |
| PBTL/SCL | 9 | DI | Weak Pull-Down | Dual function terminal that functions as an I²C clock input terminal in I²C Control Mode or configures the device to operate in pre-filter Parallel Bridge Tied Load (PBTL) mode when in Hardware Control Mode |
| PGND | 22, 27 | G | - | Ground for power device circuitry (NOTE: This terminal should be connected to the system ground) |
| PVDD | 21, 28 | P | - | Power Supply for internal power circuitry |
| SCLK | 15 | DI | Weak Pull-Down | Bit clock for the digital signal that is active on the serial data port's input data line |
| SDIN | 16 | DI | Weak Pull-Down | Data line to the serial data port |
| SFT_CLIP | 2 | AI | - | Sets the maximum output voltage before clipping |
| SPK_FAULT | 6 | DO | Open Drain | Fault terminal, which is pulled LOW when an internal fault occurs |
| SPK_GAIN0 | 11 | DI | Weak Pull-Down | Adjusts the LSB of the multi-bit gain of the speaker amplifier |
| SPK_GAIN1 | 12 | DI | Weak Pull-Down | Adjusts the MSB of the multi-bit gain of the speaker amplifier |
| SPK_SLEEP/ADR | 13 | DI | Weak Pull-Up | Places the speaker amplifier in mute |
| SPK_OUTA– | 26 | AO | - | Negative terminal for differential speaker amplifier output A |
| SPK_OUTA+ | 29 | AO | - | Positive terminal for differential speaker amplifier output A |
| SPK_OUTB– | 23 | AO | - | Negative terminal for differential speaker amplifier output B |
| SPK_OUTB+ | 20 | AO | - | Positive terminal for differential speaker amplifier output B |
| SPK_SD | 7 | DI | - | Places the device in shutdown when pulled LOW |
| VCOM | 4 | P | - | Bias voltage for internal PWM conversion block |
| PowerPAD™ | - | G | - | Provides both electrical and thermal connection from the device to the board. A matching ground pad must be provided on the PCB and the device connected to it via solder |