JAJSI95 December 2019 TL16C750E
PRODUCTION DATA.
The transmitter circuitry checks CTS before sending the next data byte. When CTS is active, the transmitter sends the next byte. To stop the transmitter from sending the following byte, CTS must be deasserted before the middle of the last stop bit that is currently being sent. The auto-CTS function reduces interrupts to the host system. When flow control is enabled, the CTS state changes and need not trigger host interrupts because the device automatically controls its own transmitter. Without auto-CTS, the transmitter sends any data present in the transmit FIFO and a receiver overrun error can result. Figure 21 shows CTS functional timing, and Figure 22 shows an example of autoflow control.
Figure 22. Autoflow Control (Auto-RTS and Auto-CTS) Example