JAJSI95 December 2019 TL16C750E
PRODUCTION DATA.
This 8-bit register provides information about the current state of the control lines from the modem, data set, or peripheral device to the processor. It also indicates when a control input from the modem changes state. Table 18 shows modem status register bit settings.
| BIT | BIT SETTINGS |
|---|---|
| 0 | Indicates that CTS input (or MCR[1] in loopback) has changed state. Cleared on a read. |
| 1 | Indicates that DSR input (or MCR[0] in loopback) has changed state. Cleared on a read. |
| 2 | Indicates that RI input (or MCR[2] in loopback) has changed state from low to high. Cleared on a read. |
| 3 | Indicates that CD input (or MCR[3] in loopback) has changed state. Cleared on a read. |
| 4 | This bit is equivalent to MCR[1] during local loop-back mode. It is the complement to the CTS input. |
| 5 | This bit is equivalent to MCR[0] during local loop-back mode. It is the complement to the DSR input. |
| 6 | This bit is equivalent to MCR[2] during local loop-back mode. It is the complement to the RI input. |
| 7 | This bit is equivalent to MCR[3] during local loop-back mode. It is the complement to the CD input. |