JAJSOO8B june 2022 – june 2023 AM620-Q1 , AM623 , AM625 , AM625-Q1
PRODUCTION DATA
The MCU_M4FSS is an Arm® Cortex®-M4F based subsystem that can run safety processing or be used as a general purpose MCU. During the boot process, the MCU_M4FSS will be configured by an initial software running on a different core. Following configuration, software will release the safety processor (M4F) out of reset, and at this point safety processor code or general purpose code can start execution.
The Cortex-M4F processor is a Cortex-M4 processor that includes the optional floating point unit (FPU) extension.
For more information, see Cortex-M4F Subsystem section in Processors and Accelerators chapter in the device TRM.