JAJSVG2 October 2024 DLPA3082
PRODUCTION DATA
Fault conditions for several supplies can be observed such as the low voltage supplies SUPPLY_FAULT (0x0C, bit 7). DMD_FAULT (0x0C, bit 4) monitors the correct function of the DMD block. The PROJ_ON_INT (0x0C, bit 5) indicates if PROJ_ON was asserted.