JAJSVM5E August 2004 – December 2024 OPA2830
PRODUCTION DATA
The maximum desired junction temperature sets the maximum allowed internal power dissipation. Do not exceed the maximum junction temperature of 150°C.
The operating junction temperature (TJ) is given by TA + PD × θJA. The total internal power dissipation (PD) is the sum of quiescent power (PDQ) and additional power dissipated in the output stage (PDL) to deliver load power. Quiescent power is the specified no-load supply current times the total supply voltage across the device. PDL depends on the required output signal and load; however, for resistive loads connected to mid-supply (VS/2), PDL is at a maximum when the output is fixed at a voltage equal to VS/4 or 3VS/4. Under this condition, PDL = VS2 / (16 × RL), where RL includes feedback network loading.
The power in the output stage, and not into the load, determines internal power dissipation.
As a worst-case example, compute the maximum TJ using an OPA2830 (VSSOP-8 package) in the circuit of Figure 8-3 operating at the maximum specified ambient temperature of 85°C and driving a 150Ω load at 2.5VDC on both outputs.
PD = 10V × 11.9mA + 2 × [52 / (16 × (150Ω || 1500Ω))] = 142mW
Maximum TJ = +85°C + (0.142W × 122.6°C/W) = 102.5°C.
Although this result is still much less than the specified maximum junction temperature, system reliability considerations require lower junction temperatures. The highest possible internal dissipation occurs if the load requires current to be forced into the output at high output voltages or sourced from the output at low output voltages. This configuration forces a high current through a large internal voltage drop in the output transistors.