JAJSW71 February 2025 ADC3683-EP , ADC3683-SEP
PRODUCTION DATA
In this mode, both the current and the previous sample have to be used in the address space as shown in Figure 7-43. The address order is different for 14/18-bit and 16/20-bit.
In the following example (Figure 7-44), the 16-bit 2-wire serial output is reordered to where lane DA1/DB1 carries the 8 MSB and lane DA0/DB0 carries 8 LSBs.