JAJU617A October 2018 – May 2022
After the number of required lumens has been determined from HUD eyebox and FOV parameters, as discussed in Section 2.4.1, details about the PGU design can be considered. Two key factors that influence PGU lumens output are the LED part selection and the optical aperture f/# in the illumination path and projection lens.
For a DLP technology based PGU, high brightness projection LEDs are often required. While larger LEDs will output more lumens, it does not necessarily mean they are the best choice at a system level. It is important to choose the best LEDs for every application. The key considerations for LED choice include: