SBAA395B May 2022 – December 2023 PCMD3140 , TLV320ADC3120 , TLV320ADC3140 , TLV320ADC5120 , TLV320ADC5140 , TLV320ADC6120 , TLV320ADC6140
By using the advantages of the analog microphones with Texas Instruments’ TLV320ADC51x0/PCM51x0-Q1 system that brings in the far-field application, quantization noise density due to the modulation improves, which brings up the height to the DR system. This leads to the near perfection of the voice recognition system that far-field application requires. The TLV320ADC51x0/PCM51x0-Q1 is an analog or digital microphone input used for an audio analog-to-digital converter that can be designed to be accommodated as needed.