SBAA483 February 2021 ADS1120 , ADS112C04 , ADS112U04 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1220 , ADS122C04 , ADS122U04 , ADS124S06 , ADS124S08 , ADS125H02 , ADS1260 , ADS1261 , ADS1262 , ADS1263
Similar to the 2-wire RTD configurations, a wire break can be detected in a one-IDAC, 3-wire RTD system in most cases just by reading the VREF monitor. Figure 3-2 shows that the IDAC current has no return path to ground when lead 1 (shown in Figure 3-2a) or lead 3 (shown in Figure 3-2b) breaks. In these cases, the VREF monitor identifies a fault.
Figure 3-2 Lead 1 (left) and Lead 3
(right) Break in a One-IDAC, 3-Wire RTD System
Lead 2 can also be broken in any case shown in Figure 3-2, but would have to be verified separately from the VREF flag and is discussed in Section 3.2.1.1 and Section 3.2.1.1.1. These conclusions are true for measurements using both a low-side and high-side RREF, even though Figure 3-2 shows low-side RREF configurations only.