SBAU456 September 2024
This section details the installation and operation of the ADS9212EVM software graphical user interface (GUI). This software requires the TSWDC155EVM (sold separately) controller to operate. The first step to installing the software is to download the latest version of the EVM GUI installer as per Table 3-1. See Figure 3-1.
| EVM | Software Download Link |
|---|---|
| ADS9212EVM | ADS9212EVM-GUI |
Accept all the license agreements and choose the destination location, project directory, and start menu. Typically, the default values work, but these values can be customized as needed based on the user's requirements.
Figure 3-1 Initial Software InstallationNext, the installer prompts the user to create a desktop icon and summarize the installation plan. Clicking Install begins copying software onto the computer. This process takes a few minutes. At completion, the user can launch a readme text file and the application. These steps are shown in Figure 3-2.
Figure 3-2 Installation Process