SBAU491 May 2025 ADS9326 , ADS9327
The INL/DNL tool measures the linearity of the of the ADS9327EVM by applying a full-scale, low-distortion sinusoidal input signal. The accuracy of the INL/DNL tool improves as the number of hits per code increases, at the cost of extra test time. Select the channel to measure the hits per code. An input signal greater than full-scale, like +0.1dBFS, is required to verify that all ADC codes are tested. Press the GET INL/DNL button to run the INL/DNL tool, as shown in Figure 3-7.